Group GPIO input interrupt / available ports

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Group GPIO input interrupt / available ports

1,064 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgrobety on Wed May 20 02:05:42 MST 2015
Hi,

I'm using the GINT0 (Group GPIO input interrupt) and want to trigger input change on GPIO. It works well with ports 0 and 1, but not on port 2.

Writing 0xFFFFFFFF to the PORT_ENA2 register read back as 0x00000000. Does it mean that the port 2 in not supported by the GINT ?

The user manual (UM10736 rev 1.1) does not show any limitation with port 2.
标签 (1)
0 项奖励
回复
0 回复数