Group GPIO input interrupt / available ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Group GPIO input interrupt / available ports

1,094件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgrobety on Wed May 20 02:05:42 MST 2015
Hi,

I'm using the GINT0 (Group GPIO input interrupt) and want to trigger input change on GPIO. It works well with ports 0 and 1, but not on port 2.

Writing 0xFFFFFFFF to the PORT_ENA2 register read back as 0x00000000. Does it mean that the port 2 in not supported by the GINT ?

The user manual (UM10736 rev 1.1) does not show any limitation with port 2.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)