GUI flash tool for programming LPC4367, LPC54xx and MKE04 controllers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI flash tool for programming LPC4367, LPC54xx and MKE04 controllers

5,411 Views
gauravmore
Contributor III

Hi, we are using LPC4367 controller in one of my development. for development we are using mcuxpresso IDE and in that we are using GUI flash tool for programming above mentioned controllers, I query is , do we have separated exe of GUI flash tool similar to flash magic tool in order to program the controllers ( LPC43XX, LPC546XX, MKE04 and MK22 series)? since we need this for our programming purpose where we will be programming multiple controllers and it will be better to use just a tool instead of a complete IDE to just program the controllers. Please let me know so that i can down load the same and test the same at my side.

Thanks,

Gaurav More

0 Kudos
Reply
5 Replies

5,386 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Now our recommended flash programming tool is FlashMagic

https://www.flashmagictool.com/

 

Have a nice day,

Jun Zhang

0 Kudos
Reply

5,376 Views
gauravmore
Contributor III

Hi Jun Zhang,

Thanks for the reply,

I downloaded the latest version of the flash magic tool for the link you sent. I check for the controller support. I cannot found the  support for MKE04 and MK22 series controllers. 

Also regarding the LPC4367 controller, also not available instead it shows LPC4337 controller.

 

Please suggest the tool and the solution for the same.

Thanks,

Gaurav More

 

 

0 Kudos
Reply

5,366 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Flash Magic only works for LPC.  I just checked LPC4367 is not included. 

I suggest considering LPCScrypt. But LPCScrypt is a command-line based

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscr...

Kinetis use blhost.exe for programming. P&E has standalone GUI but it is not free

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320138&productTab=1

 

Have a nice day,

Jun Zhang

 

 

0 Kudos
Reply

5,398 Views
converse
Senior Contributor V

NXP have not supplied a separate installer for the GUI Flash tool - there are many more components than you think, so it is very difficult to extract from the IDE.

Why don't you use Flash Magic?

Or, as an alternative, use one of the command line programming tools, such as mxil - http://www.windscooting.com/softy/mxli.html

 

5,381 Views
gauravmore
Contributor III

Hi Con Verse,

Thanks for the reply . But does the flash magic support for programming LPC4367? since it is a tricore controller.

 

Thanks 

Gaurav More

0 Kudos
Reply