GPIO ports in LQFP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO ports in LQFP100

1,690 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Tue Jun 03 07:11:09 MST 2014
Hi,

On page 440 of UM10503, the chapter on LPC43xx GPIO indicates there are no GPIO pins for the LQFP100 version.

This is surely wrong since at least P1_0 - P1_20 are available on the LPC Link2 card.

Please can you correct the manual as this is confusing.

Thanks in advance,

JohnR.

Labels (1)
0 Kudos
Reply
4 Replies

1,668 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Tue Jun 03 08:30:14 MST 2014
Hi,

Thanks.

I guess my post was due to wishful thinking that NXP would release a LQFP version ??

JohnR.
0 Kudos
Reply

1,668 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Tue Jun 03 08:26:21 MST 2014
Hi,

Thanks  - I don't know what I was thinking when I wrote that.

JohnR
0 Kudos
Reply

1,668 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Tue Jun 03 08:03:41 MST 2014
Apparently they planned to, but it was removed in Version 1.1 of the user manual (see the change notes). Apart from GPIO there are also some remnants at the start of the EMC chapter.
0 Kudos
Reply

1,668 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jun 03 07:22:16 MST 2014
Eh?

My Link2 has a 100BGA package, not LQFP. I'm not sure they have even release an LQFP100 package...
0 Kudos
Reply