GPIO interrupt delay on LPC 1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO interrupt delay on LPC 1769

1,685件の閲覧回数
romainhuet
Contributor I

Hello everybody,

I'm new here and I have a small problem with the GPIO interrupt ( LPC 1769). I manage to run the "Pinint.c" program, both with rising or falling edge. But i would like to know if it's normal to have a constant 1.5 micro second delay between the edge of my signal and the start of the handler. I just switch on a led in the interruption program and i can see that the led is on 1.5 microsecond after the edge of my signal.

It seems long and i would like to decrease that but it's like it cannot be shortened. What is the reason of that delay? I read that this GPIO is asynchronous so it should be shorter that a microsecond, isn't it?

Sorry for my english, hoping i'm understandable!

Romain

タグ(2)
0 件の賞賛
返信
1 返信

1,503件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信