Forgotten CAN-Register Struct in LPCXpresso LPC11C24 LPCOpen V2.00a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Forgotten CAN-Register Struct in LPCXpresso LPC11C24 LPCOpen V2.00a

960 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Mar 12 06:06:59 MST 2014
Somehow I'm missing the CAN-Register struct 

CAN-Base address is defined in chip.h:

#define LPC_CAN0_BASE             0x40050000

but nothing else  :quest:

Something like:
/*------------- CAN Controller (CAN) ----------------------------*/
/** @addtogroup LPC11xx_CAN LPC11xx Controller Area Network(CAN)
  @{
*/
typedef struct
{
  __IO uint32_t CNTL;/* 0x000 */
  __IO uint32_t STAT;
  __IO uint32_t EC;
  __IO uint32_t BT;
  __IO uint32_t INT;
  __IO uint32_t TEST;
  __IO uint32_t BRPE;
       uint32_t RESERVED0;
  __IO uint32_t IF1_CMDREQ;/* 0x020 */
  __IO uint32_t IF1_CMDMSK;
  __IO uint32_t IF1_MSK1;
  __IO uint32_t IF1_MSK2;
  __IO uint32_t IF1_ARB1;
  __IO uint32_t IF1_ARB2;
  __IO uint32_t IF1_MCTRL;
  __IO uint32_t IF1_DA1;
  __IO uint32_t IF1_DA2;
  __IO uint32_t IF1_DB1;
  __IO uint32_t IF1_DB2;
       uint32_t RESERVED1[13];
  __IO uint32_t IF2_CMDREQ;/* 0x080 */
  __IO uint32_t IF2_CMDMSK;
  __IO uint32_t IF2_MSK1;
  __IO uint32_t IF2_MSK2;
  __IO uint32_t IF2_ARB1;
  __IO uint32_t IF2_ARB2;
  __IO uint32_t IF2_MCTRL;
  __IO uint32_t IF2_DA1;
  __IO uint32_t IF2_DA2;
  __IO uint32_t IF2_DB1;
  __IO uint32_t IF2_DB2;
       uint32_t RESERVED2[21];
  __I  uint32_t TXREQ1;/* 0x100 */
  __I  uint32_t TXREQ2;
       uint32_t RESERVED3[6];
  __I  uint32_t ND1;/* 0x120 */
  __I  uint32_t ND2;
       uint32_t RESERVED4[6];
  __I  uint32_t IR1;/* 0x140 */
  __I  uint32_t IR2;
       uint32_t RESERVED5[6];
  __I  uint32_t MSGV1;/* 0x160 */
  __I  uint32_t MSGV2;
       uint32_t RESERVED6[6];
  __IO uint32_t CLKDIV;/* 0x180 */
} LPC_CAN0_TypeDef;
/*@}*/ /* end of group LPC11xx_CAN */

#define LPC_CAN0          ((LPC_CAN0_TypeDef    *) LPC_CAN0_BASE)
 
Labels (1)
0 Kudos
Reply
1 Reply

900 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Tue Apr 29 06:44:23 MST 2014
I think in chip.h only
#define LPC_CAN0  ((LPC_CAN0_TypeDef *) LPC_CAN0_BASE)
should appear.
The rest of your posting should be in a file named
can_11xx.h
which doesn't exist (yet?).
Obviously there is only a
ccand_11xx.h
for the CANOpen stuff (ROM driver).
0 Kudos
Reply