LPCOpen LPC15xx v2.08b release (Released: 04/10/2014) without CAN samples?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen LPC15xx v2.08b release (Released: 04/10/2014) without CAN samples?

748 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Apr 11 02:47:20 MST 2014
44 days after official chip release there's still no sign of CAN samples?

http://www.lpcware.com/content/project/lpcopen-software-development-platform-nxp-lpc-microcontroller...

That's not a known issue?


Quote:
Known issues (Carried forward)

    -LPCOpen PMU Driver will not differentiate Deep Sleep mode from Powerdown mode
    -CLKOUT example might not output any clock when it is sourced by Watchdog or RTC oscillator
    -DMA memory transfers are slower than memcpy()
    -IAR tools are able to build and flash the LPCOpen LPC15xx examples, but the IAR debugger is not yet working


Last sign of life is 35 days old...


Quote:
Fri, 2014-03-07 15:34

Hi,

The LPC15xx has ROM-based CAN support. An LPCOpen CAN example demonstrating the use of the ROM CAN support is scheduled for end of this month. Sorry for the delay.

-lpcadmin



Any hints what's going on here?
标签 (1)
0 项奖励
回复
0 回复数