For using LPC1812, any code protection for SPI Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For using LPC1812, any code protection for SPI Flash

1,120件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jason Wong on Sun Jun 15 19:44:20 MST 2014
For using LPC1812, any code protection for SPI Flash?
ラベル(1)
0 件の賞賛
返信
1 返信

1,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sun Jun 15 20:07:15 MST 2014
Hi Jason,
The NXP CRP (code read protection) does not apply to external SPI flash and there is option is most of the SPI flash for write protection.
0 件の賞賛
返信