LPC1857 MII and SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1857 MII and SD Card

981 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by REO on Wed Feb 18 09:03:41 MST 2015
Hi all

I'm currently designing an application with the LPC1857 uC.

I need both Ethernet and a SD card reader, but since the PHY we have on stock roght now only support MII I have a problem.
It turns out that MII signal "RX_CLK" is shared with SD card signal "SD_CLK" on PC_0 (pin D4 on 256 pin BGA)

Is there any kind of work around for this? Or is my only option to find a PHY that supports RMII?

Regards Rasmus
Labels (1)
0 Kudos
Reply
1 Reply

962 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Mar 17 04:54:10 MST 2015
Yes, this is the only option. Use a PHY which supports RMII.
Using MII and the SD Card interface is not possible due to this pin conflict.

Regards,
NXP Support Team
0 Kudos
Reply