Flexcomm serial single pin TXD usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexcomm serial single pin TXD usage

Jump to solution
1,444 Views
pejo
Contributor III

Hi there,

I don't have much experience in configuring Flexcomm and pin ports for LPC5504. I have the pin FC3_TXD_SCL_MISO_WS available but the rest of the FC3 serial port pins are being used as simple PIO/ Digital Input Output pins (Function=0).

I was wondering if it is possible to use only the Flexcomm 3 TXD pin for  communication (basically sending debug information) while keeping the rest of the pins for other functions like DIO.

0 Kudos
Reply
1 Solution
1,429 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pejo 

Yes, you can use only the FC3_TXD pin for communication while keeping the other Flexcomm 3 (FC3) pins as GPIO. The LPC5504 allows configuring individual pins for different functions within the Flexcomm peripheral, so you don’t need to enable the full UART interface.

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
1,430 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @pejo 

Yes, you can use only the FC3_TXD pin for communication while keeping the other Flexcomm 3 (FC3) pins as GPIO. The LPC5504 allows configuring individual pins for different functions within the Flexcomm peripheral, so you don’t need to enable the full UART interface.

BR

Harry

0 Kudos
Reply