Flashing LPC43xx and SPIFI using OpenOCD now works on Big Endian architectures

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing LPC43xx and SPIFI using OpenOCD now works on Big Endian architectures

686 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Wed Oct 23 11:03:46 MST 2013
If you have problems getting OpenOCD to work with SPIFI, and your computer has a Big Endian architecture, such as PowerPC, M68xxx or ARM in Big Endian mode, the trouble might be over soon.

The current HEAD version of OpenOCD (0.8.0) has the Big Endian problems fixed.
Furthermore, the SPIFI flashing problems have been fixed.
The LPC43xx flashing problems have been fixed.

This is tested on a PowerMac G5. To build a PPC version, you'll need to update your autotools, install pkg-config; then you should be able to build OpenOCD without problems.
Eg. if you can't ./bootstrap, update your autotools and make sure you have pkg-config installed.
标签 (1)
0 项奖励
回复
0 回复数