Flash from Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash from Android

1,460 Views
wolfgangschmidt
Contributor II

Hello,

ATM we are using LPC1769 together with an FTDI Chip to provide an USB port.

Over this port we also flash the firmware as HEX-file (virtual COM Port) in Windows.

Now we are asked wether it is possible to flash production devices with an android tablet.

As long as the Android system has USB-OTG we could connect to the LPC and send e.g. serial commands.

The question is: is there any flash tool available to flash an LPC from an Android device? (A HEX "Uploader")

Best regards

Labels (3)
0 Kudos
Reply
1 Reply

1,381 Views
soledad
NXP Employee
NXP Employee

Hi, 

No, unfortunately we don't have any Android tool available to flash an LPC.

Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply