Flash Write operations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash Write operations

跳至解决方案
2,375 次查看
WorkerEmbedded
Contributor II

Hi everybody!

I've got just a little question about the LPC micro... How much write operation can i do on the LPC55S69 MCU Flash?

Let me know, thanks!

标记 (1)
0 项奖励
回复
1 解答
2,355 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.pngxiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,356 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.pngxiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

0 项奖励
回复
2,351 次查看
frank_m
Senior Contributor III

> The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

Emphasis here on "at least".
This number is guaranteed by the vendor under worst-case conditions, which basically means maximal temperature.
At room temperature, devices might easily hold up two orders of magnitude more cycles.

But for for commercial durability calculations, you can't count on that.

0 项奖励
回复