Flash Write operations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Write operations

ソリューションへジャンプ
2,518件の閲覧回数
WorkerEmbedded
Contributor II

Hi everybody!

I've got just a little question about the LPC micro... How much write operation can i do on the LPC55S69 MCU Flash?

Let me know, thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
2,498件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,498件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

0 件の賞賛
返信
2,494件の閲覧回数
frank_m
Senior Contributor III

> The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

Emphasis here on "at least".
This number is guaranteed by the vendor under worst-case conditions, which basically means maximal temperature.
At room temperature, devices might easily hold up two orders of magnitude more cycles.

But for for commercial durability calculations, you can't count on that.

0 件の賞賛
返信