Flash Write operations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Write operations

Jump to solution
2,399 Views
WorkerEmbedded
Contributor II

Hi everybody!

I've got just a little question about the LPC micro... How much write operation can i do on the LPC55S69 MCU Flash?

Let me know, thanks!

Tags (1)
0 Kudos
Reply
1 Solution
2,379 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.pngxiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

View solution in original post

0 Kudos
Reply
2 Replies
2,380 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

I copy it from data sheet of LPC556x.

xiangjun_rong_0-1705029318387.pngxiangjun_rong_0-1705029318387.png

Hope it is helpful

BR

XiangJun Rong

 

0 Kudos
Reply
2,375 Views
frank_m
Senior Contributor III

> The on-chip flash of LPC5569/LPC55S69 can be erased/programmed about at least 100000 cycles.

Emphasis here on "at least".
This number is guaranteed by the vendor under worst-case conditions, which basically means maximal temperature.
At room temperature, devices might easily hold up two orders of magnitude more cycles.

But for for commercial durability calculations, you can't count on that.

0 Kudos
Reply