Flash LPC55s36 with OpenOCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash LPC55s36 with OpenOCD

8,285件の閲覧回数
rolandgroza
Contributor II

Hi,

I'm trying to flash a LPC55s36 MCU using OpenOCD, but it seems like the reset step is failing and I'm not sure where to go from there.

 

OpenOCD does not support the board yet, but there is a pull request (https://review.openocd.org/c/openocd/+/6800?tab=comments)  which adds support for a similar board. So I have taken that config and adapted to LPC55s36.

source [find target/swj-dp.tcl]

if { [info exists CHIPNAME] } {
	set _CHIPNAME $CHIPNAME
} else {
	set _CHIPNAME lpc55s36
}

#
# JTAG mode TAP
#
if { [info exists M33_JTAG_TAPID] } {
	set _JTAG_TAPID $M33_JTAG_TAPID
} else {
	set _JTAG_TAPID 0x4ba00477
}

#
# SWD mode TAP
#
if { [info exists M33_SWD_TAPID] } {
	set _SWD_TAPID $M33_SWD_TAPID
} else {
#	set _SWD_TAPID 0x2ba01477
	set _SWD_TAPID 0x0be12477
	#set _SWD_TAPID 0x410fd214
}

if { [using_jtag] } {
	set _CPUTAPID $_JTAG_TAPID
} {
	set _CPUTAPID $_SWD_TAPID
}

swj_newdap $_CHIPNAME m4 -irlen 4 -ircapture 0x1 -irmask 0xf \
				-expected-id $_CPUTAPID
dap create $_CHIPNAME.m4.dap -chain-position $_CHIPNAME.m4
target create $_CHIPNAME.m4 cortex_m -dap $_CHIPNAME.m4.dap

# LPCSSS36-EVK has 112 KB SRAM
if { [info exists WORKAREASIZE] } {
	set _WORKAREASIZE $WORKAREASIZE
} else {
	set _WORKAREASIZE 0x1C000
}
$_CHIPNAME.m4 configure -work-area-phys 0x20000000 \
			-work-area-size $_WORKAREASIZE -work-area-backup 0

#if {![using_hla]} {
#   # on this CPU we should use VECTRESET to perform a soft reset and
#   # manually reset the periphery
#   # SRST or SYSRESETREQ disable the debug interface for the time of
#   # the reset and will not fit our requirements for a consistent debug
#   # session
#   cortex_m reset_config vectreset
#}

cortex_m reset_config sysresetreq
adapter speed 400

#adapter srst delay 100
#adapter srst pulse_width 100
#reset_config  srst_nogate

# reset_config srst_only

 

Then running with:

sudo openocd -d -f interface/cmsis-dap.cfg -f lpc55s36.cfg -c "program [FILE] verify reset exit"

 

And eventually getting:

Open On-Chip Debugger 0.12.0
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
User : 3 3 options.c:52 configuration_output_handler(): debug_level: 3
User : 4 4 options.c:52 configuration_output_handler(): 
Debug: 5 4 options.c:233 add_default_dirs(): bindir=/usr/bin
Debug: 6 4 options.c:234 add_default_dirs(): pkgdatadir=/usr/share/openocd
Debug: 7 4 options.c:235 add_default_dirs(): exepath=/usr/bin
Debug: 8 4 options.c:236 add_default_dirs(): bin2data=../share/openocd
Debug: 9 4 configuration.c:33 add_script_search_dir(): adding /root/.config/openocd
Debug: 10 4 configuration.c:33 add_script_search_dir(): adding /root/.openocd
Debug: 11 4 configuration.c:33 add_script_search_dir(): adding /usr/bin/../share/openocd/site
Debug: 12 4 configuration.c:33 add_script_search_dir(): adding /usr/bin/../share/openocd/scripts
Debug: 13 4 command.c:155 script_debug(): command - ocd_find interface/cmsis-dap.cfg
Debug: 14 4 configuration.c:88 find_file(): found /usr/bin/../share/openocd/scripts/interface/cmsis-dap.cfg
Debug: 15 4 command.c:155 script_debug(): command - adapter driver cmsis-dap
Debug: 16 5 command.c:155 script_debug(): command - ocd_find ./config//lpc55s36.cfg
Debug: 17 5 configuration.c:88 find_file(): found ./config//lpc55s36.cfg
Debug: 18 5 command.c:155 script_debug(): command - ocd_find target/swj-dp.tcl
Debug: 19 5 configuration.c:88 find_file(): found /usr/bin/../share/openocd/scripts/target/swj-dp.tcl
Debug: 20 5 command.c:155 script_debug(): command - transport select
Info : 21 5 transport.c:265 jim_transport_select(): auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
Debug: 22 5 command.c:155 script_debug(): command - transport select
Debug: 23 5 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 24 5 command.c:155 script_debug(): command - transport select
Debug: 25 5 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 26 5 command.c:155 script_debug(): command - transport select
Debug: 27 5 command.c:155 script_debug(): command - expr  [ string first "swd" $_TRANSPORT ] != -1 
Debug: 28 5 command.c:155 script_debug(): command - swd newdap lpc55s36 m4 -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0x410fd214
Debug: 29 5 tcl.c:557 jim_newtap_cmd(): Creating New Tap, Chip: lpc55s36, Tap: m4, Dotted: lpc55s36.m4, 8 params
Debug: 30 6 core.c:1474 jtag_tap_init(): Created Tap: lpc55s36.m4 @ abs position 0, irlen 0, capture: 0x0 mask: 0x0
Debug: 31 6 command.c:155 script_debug(): command - dap create lpc55s36.m4.dap -chain-position lpc55s36.m4
Debug: 32 6 command.c:155 script_debug(): command - target create lpc55s36.m4 cortex_m -dap lpc55s36.m4.dap
Debug: 33 6 command.c:289 register_command(): command 'tpiu' is already registered
Debug: 34 6 command.c:289 register_command(): command 'rtt' is already registered
Debug: 35 6 command.c:155 script_debug(): command - lpc55s36.m4 configure -work-area-phys 0x20000000 -work-area-size 0x1C000 -work-area-backup 0
Debug: 36 6 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 37 6 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 38 6 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 39 6 command.c:155 script_debug(): command - cortex_m reset_config sysresetreq
Debug: 40 6 command.c:155 script_debug(): command - adapter speed 400
Debug: 41 6 adapter.c:251 adapter_config_khz(): handle adapter khz
Debug: 42 6 adapter.c:215 adapter_khz_to_speed(): convert khz to adapter specific speed value
Debug: 43 6 adapter.c:215 adapter_khz_to_speed(): convert khz to adapter specific speed value
User : 44 6 options.c:52 configuration_output_handler(): adapter speed: 400 kHz
User : 45 6 options.c:52 configuration_output_handler(): 
Debug: 46 7 command.c:155 script_debug(): command - init
Debug: 47 7 command.c:155 script_debug(): command - target init
Debug: 48 7 command.c:155 script_debug(): command - target names
Debug: 49 7 command.c:155 script_debug(): command - lpc55s36.m4 cget -event gdb-flash-erase-start
Debug: 50 7 command.c:155 script_debug(): command - lpc55s36.m4 configure -event gdb-flash-erase-start reset init
Debug: 51 7 command.c:155 script_debug(): command - lpc55s36.m4 cget -event gdb-flash-write-end
Debug: 52 7 command.c:155 script_debug(): command - lpc55s36.m4 configure -event gdb-flash-write-end reset halt
Debug: 53 7 command.c:155 script_debug(): command - lpc55s36.m4 cget -event gdb-attach
Debug: 54 7 command.c:155 script_debug(): command - lpc55s36.m4 configure -event gdb-attach halt 1000
Debug: 55 7 target.c:1657 handle_target_init_command(): Initializing targets...
Debug: 56 7 semihosting_common.c:109 semihosting_common_init():  
Debug: 57 35 cmsis_dap_usb_bulk.c:170 cmsis_dap_usb_open(): enumerating interfaces of 0x1d6b:0x0002
Debug: 58 63 cmsis_dap_usb_bulk.c:170 cmsis_dap_usb_open(): enumerating interfaces of 0x1d6b:0x0003
Debug: 59 65 cmsis_dap_usb_bulk.c:150 cmsis_dap_usb_open(): found product string of 0x1fc9:0x0143 'MCU-LINK on-board (r0C7) CMSIS-DAP V2.245'
Debug: 60 65 cmsis_dap_usb_bulk.c:170 cmsis_dap_usb_open(): enumerating interfaces of 0x1fc9:0x0143
Debug: 61 65 cmsis_dap_usb_bulk.c:217 cmsis_dap_usb_open(): found interface 0 string 'MCU-LINK on-board (r0C7) CMSIS-DAP V2.245'
Debug: 62 65 cmsis_dap_usb_bulk.c:237 cmsis_dap_usb_open(): skipping interface 0, endpoint[0] is not bulk out
Debug: 63 66 cmsis_dap_usb_bulk.c:237 cmsis_dap_usb_open(): skipping interface 1, endpoint[0] is not bulk out
Debug: 64 67 cmsis_dap_usb_bulk.c:230 cmsis_dap_usb_open(): skipping interface 2, has only 1 endpoints
Debug: 65 67 cmsis_dap_usb_bulk.c:276 cmsis_dap_usb_open(): skipping interface 3, class 10 subclass 0 protocol 0
Debug: 66 68 cmsis_dap_usb_bulk.c:237 cmsis_dap_usb_open(): skipping interface 4, endpoint[0] is not bulk out
Debug: 67 69 cmsis_dap_usb_bulk.c:170 cmsis_dap_usb_open(): enumerating interfaces of 0x2109:0x3431
Debug: 68 71 cmsis_dap_usb_bulk.c:170 cmsis_dap_usb_open(): enumerating interfaces of 0x1d6b:0x0002
Info : 69 172 cmsis_dap.c:1027 cmsis_dap_get_caps_info(): CMSIS-DAP: SWD supported
Info : 70 172 cmsis_dap.c:1027 cmsis_dap_get_caps_info(): CMSIS-DAP: JTAG supported
Info : 71 172 cmsis_dap.c:1027 cmsis_dap_get_caps_info(): CMSIS-DAP: Atomic commands supported
Info : 72 179 cmsis_dap.c:1004 cmsis_dap_get_version_info(): CMSIS-DAP: FW Version = 1.10
Info : 73 186 cmsis_dap.c:989 cmsis_dap_get_serial_info(): CMSIS-DAP: Serial# = OKF3A0JHHR30I
Info : 74 191 cmsis_dap.c:1156 cmsis_dap_swd_open(): CMSIS-DAP: Interface Initialised (SWD)
Debug: 75 195 cmsis_dap.c:1224 cmsis_dap_init(): CMSIS-DAP: Packet Size = 1024
Debug: 76 199 cmsis_dap.c:1238 cmsis_dap_init(): CMSIS-DAP: Packet Count = 4
Debug: 77 199 cmsis_dap.c:1241 cmsis_dap_init(): Allocating FIFO for 3 pending packets
Info : 78 203 cmsis_dap.c:1060 cmsis_dap_get_status(): SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 1 TDO = 0 nTRST = 0 nRESET = 1
Info : 79 225 cmsis_dap.c:1292 cmsis_dap_init(): CMSIS-DAP: Interface ready
Debug: 80 225 adapter.c:215 adapter_khz_to_speed(): convert khz to adapter specific speed value
Debug: 81 225 adapter.c:219 adapter_khz_to_speed(): have adapter set up
Debug: 82 229 adapter.c:215 adapter_khz_to_speed(): convert khz to adapter specific speed value
Debug: 83 229 adapter.c:219 adapter_khz_to_speed(): have adapter set up
Info : 84 229 adapter.c:179 adapter_init(): clock speed 400 kHz
Debug: 85 229 openocd.c:134 handle_init_command(): Debug Adapter init complete
Debug: 86 229 command.c:155 script_debug(): command - transport init
Debug: 87 229 transport.c:219 handle_transport_init(): handle_transport_init
Debug: 88 229 command.c:155 script_debug(): command - dap init
Debug: 89 229 arm_dap.c:97 dap_init_all(): Initializing all DAPs ...
Debug: 90 229 arm_dap.c:121 dap_init_all(): DAP lpc55s36.m4 configured by default to use ADIv5 protocol
Debug: 91 237 cmsis_dap.c:1100 cmsis_dap_swd_switch_seq(): JTAG-to-SWD
Info : 92 249 adi_v5_swd.c:370 swd_connect_single(): SWD DPIDR 0x6ba02477
Debug: 93 253 arm_adi_v5.c:679 dap_dp_init(): lpc55s36.m4.dap
Debug: 94 253 arm_adi_v5.c:711 dap_dp_init(): DAP: wait CDBGPWRUPACK
Debug: 95 253 arm_adi_v5.h:638 dap_dp_poll_register(): DAP: poll 4, mask 0x20000000, value 0x20000000
Debug: 96 257 arm_adi_v5.c:719 dap_dp_init(): DAP: wait CSYSPWRUPACK
Debug: 97 257 arm_adi_v5.h:638 dap_dp_poll_register(): DAP: poll 4, mask 0x80000000, value 0x80000000
Debug: 98 261 cmsis_dap.c:808 cmsis_dap_swd_write_from_queue(): refusing to enable sticky overrun detection
Debug: 99 265 openocd.c:151 handle_init_command(): Examining targets...
Debug: 100 265 target.c:1843 target_call_event_callbacks(): target event 19 (examine-start) for core lpc55s36.m4
Debug: 101 265 arm_adi_v5.c:1095 dap_get_ap(): refcount AP#0x0 get 1
Debug: 102 269 arm_adi_v5.c:1038 dap_find_get_ap(): Found MEM-AP AHB3 at AP index: 0 (IDR=0x84770001)
Debug: 103 277 arm_adi_v5.c:825 mem_ap_init(): MEM_AP Packed Transfers: enabled
Debug: 104 277 arm_adi_v5.c:836 mem_ap_init(): MEM_AP CFG: large data 0, long address 0, big-endian 0
Debug: 105 281 target.c:2628 target_read_u32(): address: 0xe000ed00, value: 0x410fd214
Info : 106 281 cortex_m.c:2369 cortex_m_examine(): [lpc55s36.m4] Cortex-M33 r0p4 processor detected
Debug: 107 281 cortex_m.c:2384 cortex_m_examine(): [lpc55s36.m4] cpuid: 0x410fd214
Debug: 108 285 target.c:2628 target_read_u32(): address: 0xe000ef40, value: 0x10110021
Debug: 109 289 target.c:2628 target_read_u32(): address: 0xe000ef44, value: 0x11000011
Debug: 110 289 cortex_m.c:2401 cortex_m_examine(): [lpc55s36.m4] Cortex-M33 floating point feature FPv5_SP found
Debug: 111 293 target.c:2628 target_read_u32(): address: 0xe000efb8, value: 0x0000000f
Debug: 112 297 target.c:2628 target_read_u32(): address: 0xe000edf0, value: 0x01000001
Debug: 113 297 target.c:2716 target_write_u32(): address: 0xe000edfc, value: 0x01000000
Debug: 114 306 target.c:2628 target_read_u32(): address: 0xe0002000, value: 0x10000081
Debug: 115 306 target.c:2716 target_write_u32(): address: 0xe0002008, value: 0x00000000
Debug: 116 311 target.c:2716 target_write_u32(): address: 0xe000200c, value: 0x00000000
Debug: 117 315 target.c:2716 target_write_u32(): address: 0xe0002010, value: 0x00000000
Debug: 118 319 target.c:2716 target_write_u32(): address: 0xe0002014, value: 0x00000000
Debug: 119 323 target.c:2716 target_write_u32(): address: 0xe0002018, value: 0x00000000
Debug: 120 328 target.c:2716 target_write_u32(): address: 0xe000201c, value: 0x00000000
Debug: 121 333 target.c:2716 target_write_u32(): address: 0xe0002020, value: 0x00000000
Debug: 122 338 target.c:2716 target_write_u32(): address: 0xe0002024, value: 0x00000000
Debug: 123 343 cortex_m.c:2488 cortex_m_examine(): [lpc55s36.m4] FPB fpcr 0x10000081, numcode 8, numlit 0
Debug: 124 348 target.c:2628 target_read_u32(): address: 0xe0001000, value: 0x40000000
Debug: 125 348 cortex_m.c:2187 cortex_m_dwt_setup(): [lpc55s36.m4] DWT_CTRL: 0x40000000
Debug: 126 353 target.c:2628 target_read_u32(): address: 0xe0001fbc, value: 0x47701a02
Debug: 127 353 cortex_m.c:2194 cortex_m_dwt_setup(): [lpc55s36.m4] DWT_DEVARCH: 0x47701a02
Debug: 128 353 target.c:2716 target_write_u32(): address: 0xe0001028, value: 0x00000000
Debug: 129 357 target.c:2716 target_write_u32(): address: 0xe0001038, value: 0x00000000
Debug: 130 361 target.c:2716 target_write_u32(): address: 0xe0001048, value: 0x00000000
Debug: 131 365 target.c:2716 target_write_u32(): address: 0xe0001058, value: 0x00000000
Debug: 132 370 cortex_m.c:2241 cortex_m_dwt_setup(): [lpc55s36.m4] DWT dwtcr 0x40000000, comp 4, watch/trigger
Info : 133 370 cortex_m.c:2498 cortex_m_examine(): [lpc55s36.m4] target has 8 breakpoints, 4 watchpoints
Debug: 134 370 target.c:1843 target_call_event_callbacks(): target event 21 (examine-end) for core lpc55s36.m4
Debug: 135 370 command.c:155 script_debug(): command - flash init
Debug: 136 370 tcl.c:1375 handle_flash_init_command(): Initializing flash devices...
Debug: 137 370 command.c:155 script_debug(): command - nand init
Debug: 138 370 tcl.c:487 handle_nand_init_command(): Initializing NAND devices...
Debug: 139 371 command.c:155 script_debug(): command - pld init
Debug: 140 371 pld.c:194 handle_pld_init_command(): Initializing PLDs...
Debug: 141 371 command.c:155 script_debug(): command - tpiu init
Info : 142 371 gdb_server.c:3791 gdb_target_start(): starting gdb server for lpc55s36.m4 on 3333
Info : 143 371 server.c:297 add_service(): Listening on port 3333 for gdb connections
Debug: 144 371 command.c:155 script_debug(): command - reset init
Debug: 145 375 target.c:1862 target_call_reset_callbacks(): target reset 3 (init)
Debug: 146 375 command.c:155 script_debug(): command - expr [catch {ocd_process_reset_inner $MODE} result] == 0
Debug: 147 376 command.c:155 script_debug(): command - target names
Debug: 148 376 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event reset-start
Debug: 149 376 command.c:155 script_debug(): command - transport select
Debug: 150 376 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 151 376 command.c:155 script_debug(): command - transport select
Debug: 152 376 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 153 376 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event examine-start
Debug: 154 376 command.c:155 script_debug(): command - lpc55s36.m4 arp_examine allow-defer
Debug: 155 383 arm_adi_v5.c:825 mem_ap_init(): MEM_AP Packed Transfers: enabled
Debug: 156 383 arm_adi_v5.c:836 mem_ap_init(): MEM_AP CFG: large data 0, long address 0, big-endian 0
Debug: 157 383 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event examine-end
Debug: 158 383 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event reset-assert-pre
Debug: 159 383 command.c:155 script_debug(): command - transport select
Debug: 160 383 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 161 384 command.c:155 script_debug(): command - lpc55s36.m4 arp_reset assert 1
Debug: 162 384 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 163 384 cortex_m.c:1401 cortex_m_assert_reset(): [lpc55s36.m4] target->state: running, examined
Debug: 164 391 cortex_m.c:1516 cortex_m_assert_reset(): [lpc55s36.m4] Using Cortex-M SYSRESETREQ
Debug: 165 395 cmsis_dap.c:872 cmsis_dap_swd_read_process(): SWD ack not OK @ 4 FAULT
Debug: 166 395 cortex_m.c:1529 cortex_m_assert_reset(): [lpc55s36.m4] Ignoring AP write error right after reset
Debug: 167 395 arm_adi_v5.c:754 dap_dp_init_or_reconnect(): lpc55s36.m4.dap
Debug: 168 399 arm_adi_v5.c:679 dap_dp_init(): lpc55s36.m4.dap
Debug: 169 399 arm_adi_v5.c:711 dap_dp_init(): DAP: wait CDBGPWRUPACK
Debug: 170 399 arm_adi_v5.h:638 dap_dp_poll_register(): DAP: poll 4, mask 0x20000000, value 0x20000000
Debug: 171 403 cmsis_dap.c:872 cmsis_dap_swd_read_process(): SWD ack not OK @ 0 FAULT
Error: 172 403 cortex_m.c:1533 cortex_m_assert_reset(): [lpc55s36.m4] DP initialisation failed
Debug: 173 454 cortex_m.c:986 cortex_m_halt(): [lpc55s36.m4] target->state: reset
Debug: 174 454 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event reset-assert-post
Debug: 175 454 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event reset-deassert-pre
Debug: 176 454 command.c:155 script_debug(): command - transport select
Debug: 177 454 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 178 454 command.c:155 script_debug(): command - lpc55s36.m4 arp_reset deassert 1
Debug: 179 455 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 180 455 cortex_m.c:1569 cortex_m_deassert_reset(): [lpc55s36.m4] target->state: reset, examined
Debug: 181 457 core.c:640 adapter_system_reset(): SRST line released
Debug: 182 457 command.c:155 script_debug(): command - lpc55s36.m4 invoke-event reset-deassert-post
Debug: 183 458 command.c:155 script_debug(): command - transport select
Debug: 184 458 command.c:155 script_debug(): command - expr  [ string first "jtag" $_TRANSPORT ] != -1 
Debug: 185 458 command.c:155 script_debug(): command - lpc55s36.m4 was_examined
Debug: 186 458 command.c:155 script_debug(): command - lpc55s36.m4 arp_waitstate halted 1000
Debug: 187 469 cmsis_dap.c:1100 cmsis_dap_swd_switch_seq(): JTAG-to-SWD
Info : 188 481 adi_v5_swd.c:370 swd_connect_single(): SWD DPIDR 0x6ba02477
Debug: 189 485 arm_adi_v5.c:679 dap_dp_init(): lpc55s36.m4.dap
Debug: 190 485 arm_adi_v5.c:711 dap_dp_init(): DAP: wait CDBGPWRUPACK
Debug: 191 485 arm_adi_v5.h:638 dap_dp_poll_register(): DAP: poll 4, mask 0x20000000, value 0x20000000
Debug: 192 489 arm_adi_v5.c:719 dap_dp_init(): DAP: wait CSYSPWRUPACK
Debug: 193 489 arm_adi_v5.h:638 dap_dp_poll_register(): DAP: poll 4, mask 0x80000000, value 0x80000000
Debug: 194 493 cmsis_dap.c:808 cmsis_dap_swd_write_from_queue(): refusing to enable sticky overrun detection
Debug: 195 501 target.c:3286 target_wait_state(): waiting for target halted...
Debug: 196 505 cortex_m.c:921 cortex_m_poll(): [lpc55s36.m4] Exit from reset with dcb_dhcsr 0x1000001
Debug: 197 509 cortex_m.c:588 cortex_m_endreset_event(): [lpc55s36.m4] DCB_DEMCR = 0x01000501
Debug: 198 513 target.c:2716 target_write_u32(): address: 0xe0002000, value: 0x00000003
Debug: 199 521 target.c:2628 target_read_u32(): address: 0xe0002000, value: 0x10000081
Debug: 200 521 target.c:2716 target_write_u32(): address: 0xe0002008, value: 0x00000000
Debug: 201 525 target.c:2716 target_write_u32(): address: 0xe000200c, value: 0x00000000
Debug: 202 529 target.c:2716 target_write_u32(): address: 0xe0002010, value: 0x00000000
Debug: 203 533 target.c:2716 target_write_u32(): address: 0xe0002014, value: 0x00000000
Debug: 204 538 target.c:2716 target_write_u32(): address: 0xe0002018, value: 0x00000000
Debug: 205 543 target.c:2716 target_write_u32(): address: 0xe000201c, value: 0x00000000
Debug: 206 547 target.c:2716 target_write_u32(): address: 0xe0002020, value: 0x00000000
Debug: 207 551 target.c:2716 target_write_u32(): address: 0xe0002024, value: 0x00000000
Debug: 208 555 target.c:2716 target_write_u32(): address: 0xe0001020, value: 0x00000000
Debug: 209 559 target.c:2716 target_write_u32(): address: 0xe0001024, value: 0x00000000
Debug: 210 563 target.c:2716 target_write_u32(): address: 0xe0001028, value: 0x00000000
Debug: 211 567 target.c:2716 target_write_u32(): address: 0xe0001030, value: 0x00000000
Debug: 212 571 target.c:2716 target_write_u32(): address: 0xe0001034, value: 0x00000000
Debug: 213 575 target.c:2716 target_write_u32(): address: 0xe0001038, value: 0x00000000
Debug: 214 579 target.c:2716 target_write_u32(): address: 0xe0001040, value: 0x00000000
Debug: 215 583 target.c:2716 target_write_u32(): address: 0xe0001044, value: 0x00000000
Debug: 216 587 target.c:2716 target_write_u32(): address: 0xe0001048, value: 0x00000000
Debug: 217 591 target.c:2716 target_write_u32(): address: 0xe0001050, value: 0x00000000
Debug: 218 596 target.c:2716 target_write_u32(): address: 0xe0001054, value: 0x00000000
Debug: 219 601 target.c:2716 target_write_u32(): address: 0xe0001058, value: 0x00000000
Debug: 220 1005 log.c:412 gdb_timeout_warning(): keep_alive() was not invoked in the 1000 ms timelimit (1005 ms). This may cause trouble with GDB connections.
Error: 221 1505 target.c:3294 target_wait_state(): timed out while waiting for target halted
Debug: 222 1505 command.c:155 script_debug(): command - lpc55s36.m4 curstate
Debug: 223 1506 command.c:544 run_command(): Command 'reset' failed with error code -4
Debug: 224 1506 command.c:155 script_debug(): command - echo ** Unable to reset target **
User : 225 1509 command.c:685 handle_echo(): ** Unable to reset target **
Debug: 226 1509 command.c:155 script_debug(): command - shutdown error
User : 227 1513 server.c:758 handle_shutdown_command(): shutdown command invoked
Debug: 228 1513 command.c:544 run_command(): Command 'shutdown' failed with error code -4
User : 229 1514 command.c:608 command_run_line(): 
Debug: 230 1514 arm_adi_v5.c:1120 dap_put_ap(): refcount AP#0x0 put 0
Debug: 231 1514 target.c:2199 target_free_all_working_areas_restore(): freeing all working areas
Debug: 232 1522 cmsis_dap.c:1110 cmsis_dap_swd_switch_seq(): SWD-to-JTAG
Oopsies, trying again in 1 second

 

Has anyone managed to flash this board w/ OpenOCD? Otherwise, what are the alternatives given that I need to be able to programatically do it from a ARM32 Linux machine using SWD.

タグ(1)
6 返答(返信)

8,039件の閲覧回数
leannee
Contributor II

Hello @rolandgroza ! Thank you for the cfg file. I used it and have the same error. Have you managed to make it work?

0 件の賞賛
返信

8,012件の閲覧回数
rolandgroza
Contributor II

We have reached out to one of the the OpenOCD contributors and he's helped impl. the flash driver for this model: https://github.com/transcelestial/openocd. 

 

8,249件の閲覧回数
rolandgroza
Contributor II

Also, if you check https://github.com/openocd-org/openocd/blob/151b743714382120dbe0dee0e0eeb75826ef5b3a/src/flash/nor/l... are any of those impl. close enough to how the logic/algo for flashing lpc553x is? I'm thinking of modifying the source to support this chip too.

0 件の賞賛
返信

8,251件の閲覧回数
rolandgroza
Contributor II

Hi @xiangjun_rong . Thanks for sharing that. There's a note about some source code for the reference impl. which could be shared, would that be possible? And can that be used for flashing and resetting the MCU?

 

0 件の賞賛
返信

8,246件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the programming on-chip flash of LPC55s36, the ROM provides the API function to program flash.

Pls download the reference manual of LPC55S36 from the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

Refer to section 28.2.1 ROM API structure.

BTW, pls download SDK package from the link:

https://mcuxpresso.nxp.com/en/welcome

There is flash operation example

xiangjun_rong_0-1706150393943.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

8,251件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is an application note focusing on the SWD programming, pls check if it is helpful.

BR

XiangJun Rong