Firmware upgrades using a USB port as a MSC for the LPC1837/1857

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware upgrades using a USB port as a MSC for the LPC1837/1857

774 Views
andrewbarningha
Contributor III

I have been using the LPC1549, when i do firmware upgrades on this device i simply connect the device to a USB port and my PC sees the device as a MSC, i can then copy the bin file straight to the MSC.

This feature is very useful for firmware upgrades on site where the technicians do not need any special tools or applications.

Is this feature available on the LPC1837 / LPC1857?

Thanks

0 Kudos
Reply
1 Reply

658 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Andrew Barningham,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

1)Is this feature available on the LPC1837 / LPC1857?

No, these chips don't support.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply