Firmware upgrades using a USB port as a MSC for the LPC1837/1857

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware upgrades using a USB port as a MSC for the LPC1837/1857

777件の閲覧回数
andrewbarningha
Contributor III

I have been using the LPC1549, when i do firmware upgrades on this device i simply connect the device to a USB port and my PC sees the device as a MSC, i can then copy the bin file straight to the MSC.

This feature is very useful for firmware upgrades on site where the technicians do not need any special tools or applications.

Is this feature available on the LPC1837 / LPC1857?

Thanks

0 件の賞賛
返信
1 返信

661件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andrew Barningham,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

1)Is this feature available on the LPC1837 / LPC1857?

No, these chips don't support.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信