Firmware update using A/B Partion in NXP LPC54s018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware update using A/B Partion in NXP LPC54s018

1,840件の閲覧回数
robo_v
Contributor I

We would like to update the micrcontroller firmware. Can we separate the the flash to A& B partion and NXP LPC54s018 can switch Partion A or B for boot?

0 件の賞賛
返信
5 返答(返信)

1,816件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, tell me more about your application this mean that you already have the bootloader with OTA or not?

If not, the recommendation is using the next one.

MCU Bootloader | NXP Semiconductors

Pavel_Hernandez_0-1725401480738.pngPavel_Hernandez_0-1725401480738.png

Best regards,
Pavel

 

0 件の賞賛
返信

1,808件の閲覧回数
robo_v
Contributor I
Using ISP mode we are downloading the secondary bootloader to RAM and then we are updating the fw image to flash. But in this case,
If the update process did
not finish correctly it can be difficult to recover the old image. So we are looking A/B partion approach
0 件の賞賛
返信

1,787件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, just to be clear on what means A/B, are you looking for the OTA process or the recovery image?

Could you elaborate further about?

Best regards,
Pavel

0 件の賞賛
返信

1,766件の閲覧回数
robo_v
Contributor I
Yes Am looking for OTA process of updating the uC firmware. During this process even if it is interrupted or stoped in the middle it should not result in the brick/non-responsive state
0 件の賞賛
返信

1,746件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信