Firmware Image Header Creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Image Header Creation

1,636 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Tue Apr 28 22:07:05 MST 2015
Hi,

I have created a firmware image for a LPC43xx based device. I have to flash it to the SPIFI NOR on the board. Though, LPC has provided with DFUSec utility to flash the firmware due to unavoidable reasons I cannot use that utility.

So the next option with me is to flash the firmware using Flash Magic. The DFU Sec utility prepends the data with a boot image header following which we can successfully flash and execute the firmware. But the DFU Sec can add that header to a bin file

However, there is no such utility for prepend a Header to the hex file generated file, hence an image flashed to the NOR always fails to execute.

Any idea on how to add the header to the firmware?

regards,
Milind.
Labels (1)
0 Kudos
Reply
1 Reply

1,497 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Apr 28 22:42:56 MST 2015
Take a look at lpcscrypt which has a utility for doing this
http://www.lpcware.com/lpcscrypt
0 Kudos
Reply