Content originally posted in LPCWare by sipel_tp on Thu Aug 22 08:54:00 MST 2013
Hello everybody, 
I've tried to inicialize a SD card using the elm-chan.org FATFS library with a LPC1788 and the MCI interface.
I manage to recognize the card but I can't make the library work.
I've tried to inicialize a SD card like I show you right here but f_open keeps me throwing FR_NO_FILESYSTEM:
---------------------------------------------------------------------------------------
en_Mci_CardType cardType;
uint32_t i,j;
BYTE buffer[64];
FRESULT result;
static FATFS fs;       
FIL objectFIL;
memset(buffer, 0, 64);
disk_initialize(0);
result = f_mount(0, &fs);
cardType = MCI_GetCardType();
result = f_open(&objectFIL, "0:SDCARD/archive1.txt", FA_OPEN_EXISTING |FA_READ);
-----------------------------------------------------------------------------------------
Here is the part of the code inside f_open where it makes that:
----------------------------------------------------------------------------------------
fmt = check_fs(fs, bsect = 0);/* Check sector 0 as an SFD format */
if (fmt == 1) {/* Not an FAT boot record, it may be patitioned */
/* Check a partition listed in top of the partition table */
tbl = &fs->win[MBR_Table + LD2PT(vol) * 16];/* Partition table */
if (tbl[4]) {/* Is the partition existing? */
bsect = LD_DWORD(&tbl[8]);/* Partition offset in LBA */
[color=#f00]fmt = check_fs(fs, bsect);/* Check the partition */[/color]
}
}
if (fmt == 3) return FR_DISK_ERR;
[color=#00c]if (fmt || LD_WORD(fs->win+BPB_BytsPerSec) != SS(fs))/* No valid FAT patition is found */
return FR_NO_FILESYSTEM;[/color]
----------------------------------------------------------------------------------------------------------------------------
The line in red returns me fmt=2 so later in the blue line it finds that the partition is not valid.
checl_fs is in here:
--------------------------------------------------------------------------------------------------------------------
static
BYTE check_fs (/* 0:The FAT boot record, 1:Valid boot record but not an FAT, 2:Not a boot record, 3:Error */
FATFS *fs,/* File system object */
DWORD sect/* Sector# (lba) to check if it is an FAT boot record or not */
)
{
if (disk_read(fs->drive, fs->win, sect, 1) != RES_OK)/* Load boot record */
return 3;
if (LD_WORD(&fs->win[BS_55AA]) != 0xAA55)/* Check record signature (always placed at offset 510 even if the sector size is >512) */
return 2;
if ((LD_DWORD(&fs->win[BS_FilSysType]) & 0xFFFFFF) == 0x544146)/* Check "FAT" string */
return 0;
if ((LD_DWORD(&fs->win[BS_FilSysType32]) & 0xFFFFFF) == 0x544146)
return 0;
return 1;
}
--------------------------------------------------------------------------------------------------------------------------------------------------
I would extremely apreciate any kind of help,
Thank you very much !