Hello Team,
I am seeing an issue, not sure what is missing.
Please find more details,
#define SPI3_IF SPI3
#define SPI3_CLK_SRC kCLOCK_Flexcomm3
#define SPI3_CLK_FREQ CLOCK_GetFlexCommClkFreq(3U)
#define SPI3_SLAVE_SELECT 0
#define SPI3_IRQHandler FLEXCOMM3_IRQHandler
#define SPI3_IRQn FLEXCOMM3_IRQn
Below is my interrupt handler,
uint16_t receiveBuff[256];
void SPI3_IRQHandler(void)
{
uint16_t tmp_data;
PRINTF("(%s) - %s() at line %d -> START\r\n",__FILE__,__func__,__LINE__);
if ((SPI_GetStatusFlags(SPI3_IF) & kSPI_RxNotEmptyFlag))
{
tmp_data = SPI_ReadData(SPI3_IF);
receiveBuff[rxIndex] = tmp_data;
}
SDK_ISR_EXIT_BARRIER;
}
In the spi initialization,
SPI_MasterGetDefaultConfig(&masterConfig);
// Set the baudrate
masterConfig.enableLoopback = false;
masterConfig.enableMaster = true;
masterConfig.polarity = kSPI_ClockPolarityActiveHigh;
masterConfig.phase = kSPI_ClockPhaseFirstEdge;
masterConfig.direction = kSPI_MsbFirst;
masterConfig.baudRate_Bps = SPI3_BAUDRATE_500000;
masterConfig.sselNum = kSPI_Ssel0;
masterConfig.sselPol = (spi_spol_t)SPI3_SPOL;
// SPI enable and Mast mode selection is done as part of this
SPI_MasterInit(SPI3_IF, &masterConfig, SPI3_CLK_FREQ);
SPI_EnableInterrupts(SPI3_IF, kSPI_TxLvlIrq | kSPI_RxLvlIrq);
EnableIRQ(SPI3_IRQn);
But when I run the code, the control is going to "FLEXCOMM3_DriverIRQHandler", even in debug also I am seeing the same behavior. So I am wondering what is causing that.
I understand that, SDK specific interrupt handler gets invoked, only when there is any interrupt handler defined for it, but in this scenario there is an already interrupt handler defined.
Can someone please let me know, what is missing?