External debugger SWD OR J-TAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External debugger SWD OR J-TAG

Jump to solution
2,027 Views
ujwal_kumar_N_L
Contributor III

Hi Community ,

Im working on the debugger ofLPC55S69 ,trying to use the microcontroller and program it with external Debugger .

Board :LPC55S69

Debugging using SWD.

PROBLEM:

  1. Can we use the external debugger to dump the code to the microcontroller ?(Using only SWD not JLINK).
  2. Can we only use  SWCLK,SWDIO and SWO instead of the 10 pin P7 SWD .Only utilizing these 3 pins and debugging it module?
  3. Best external debugger for dumping the code .Suggestions.
  4. Steps or material regarding the above Debugging.

Thank and Regards 
UJWAL KUMAR N L

0 Kudos
Reply
1 Solution
2,017 Views
ErichStyger
Specialist I

Hello @ujwal_kumar_N_L ,

1. If you mean with 'dump the code to the microcontroller' the programming and flashing of it, then yes: you can use SWD for this. You don't have to use a J-Link, you can use any other debug probe supporting the LPC55S69, e.g. MCU-Link (Pro) or P&E Multilink.

2. You need SWCKL, SWDIO and GND. SWO is a trace pin, see https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/

3. Use a J-Link, or program the J-Link firmware on the board. Or use the NXP MCU-Link Pro or non-pro, or use a P&E Multilink. Choice depends on your needs and budget available.

4. https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-boa...

 

View solution in original post

0 Kudos
Reply
1 Reply
2,018 Views
ErichStyger
Specialist I

Hello @ujwal_kumar_N_L ,

1. If you mean with 'dump the code to the microcontroller' the programming and flashing of it, then yes: you can use SWD for this. You don't have to use a J-Link, you can use any other debug probe supporting the LPC55S69, e.g. MCU-Link (Pro) or P&E Multilink.

2. You need SWCKL, SWDIO and GND. SWO is a trace pin, see https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/

3. Use a J-Link, or program the J-Link firmware on the board. Or use the NXP MCU-Link Pro or non-pro, or use a P&E Multilink. Choice depends on your needs and budget available.

4. https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-boa...

 

0 Kudos
Reply