External debugger SWD OR J-TAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External debugger SWD OR J-TAG

ソリューションへジャンプ
2,046件の閲覧回数
ujwal_kumar_N_L
Contributor III

Hi Community ,

Im working on the debugger ofLPC55S69 ,trying to use the microcontroller and program it with external Debugger .

Board :LPC55S69

Debugging using SWD.

PROBLEM:

  1. Can we use the external debugger to dump the code to the microcontroller ?(Using only SWD not JLINK).
  2. Can we only use  SWCLK,SWDIO and SWO instead of the 10 pin P7 SWD .Only utilizing these 3 pins and debugging it module?
  3. Best external debugger for dumping the code .Suggestions.
  4. Steps or material regarding the above Debugging.

Thank and Regards 
UJWAL KUMAR N L

0 件の賞賛
返信
1 解決策
2,036件の閲覧回数
ErichStyger
Specialist I

Hello @ujwal_kumar_N_L ,

1. If you mean with 'dump the code to the microcontroller' the programming and flashing of it, then yes: you can use SWD for this. You don't have to use a J-Link, you can use any other debug probe supporting the LPC55S69, e.g. MCU-Link (Pro) or P&E Multilink.

2. You need SWCKL, SWDIO and GND. SWO is a trace pin, see https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/

3. Use a J-Link, or program the J-Link firmware on the board. Or use the NXP MCU-Link Pro or non-pro, or use a P&E Multilink. Choice depends on your needs and budget available.

4. https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-boa...

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,037件の閲覧回数
ErichStyger
Specialist I

Hello @ujwal_kumar_N_L ,

1. If you mean with 'dump the code to the microcontroller' the programming and flashing of it, then yes: you can use SWD for this. You don't have to use a J-Link, you can use any other debug probe supporting the LPC55S69, e.g. MCU-Link (Pro) or P&E Multilink.

2. You need SWCKL, SWDIO and GND. SWO is a trace pin, see https://mcuoneclipse.com/2021/05/22/swo-with-arm-cortex-m33/

3. Use a J-Link, or program the J-Link firmware on the board. Or use the NXP MCU-Link Pro or non-pro, or use a P&E Multilink. Choice depends on your needs and budget available.

4. https://mcuoneclipse.com/2019/05/18/internal-and-external-debug-options-for-the-nxp-lpc55s69-evk-boa...

 

0 件の賞賛
返信