External Clock on LPC55s06

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Clock on LPC55s06

4,362件の閲覧回数
Devaharsha
Contributor III

Hi,

We want to generate clock using external oscillator (which is 16 MHz ) and the systick handler should get an interrupted with every 100 ms. 

We have modified the code in the custom driver. The output is coming with SYS_CSR = (0x1 << 2) , which is a Processor Clock but code is going to "Hard Fault" when SYS_CSR = (0x0 << 2) , which is external clock.  

Can anyone help me in figuring out the value to be given in SYST_CSR (systick control and status register)?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,360件の閲覧回数
Badman
Contributor I

Try to clear second bit this code

SYS_CSR &= ~(0x1 << 2);
0 件の賞賛
返信

4,341件の閲覧回数
Devaharsha
Contributor III

@Badman We have tried with your solution and its working.

 

The Main clock frequency is 96 Mhz and setting SYSTICKCLKDIV0 register with zero (divide by 1). With Systick handler giving interrupt at every 100ms (calculated based on freq=96 Mhz), the code is not interrupted at the handler.  

But with setting SYSTICKCLKDIV0 register with 1 (divide by 2), we get 48 Mhz. With above 48 Mhz, and given Systick interrupt value at 100 ms (calculated based on freq = 48 Mhz), the handler is getting hit. So, we are assuming the main clock is 48 Mhz instead of 96 Mhz.

So, Can you help me in getting the reasoning why the code is not working with 96 Mhz?

 

Our modification in clock registers:

SYSCON->SYSTICKCLKDIV0 = 0x00; // systick clk divide with one
SYSCON->SYSTICKCLKSEL0 = 0x00; //selecting main clk for systick from syscon (96 MHZ)
SYSTICK->SYST_CSR |= (1 << 1); // enable interrupt to systick (100msec)
SYSTICK->SYST_CSR &= ~ (1 << 2); // enable external clk
SYSTICK->SYST_CSR |= (1 << 0); // systick counter enable

0 件の賞賛
返信