External Clock Frequency range LPC55Sxx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Clock Frequency range LPC55Sxx

ソリューションへジャンプ
2,677件の閲覧回数
Watarat
Contributor I

I am unclear as to the range of frequencies that can be applied as an external clock.
I wish to use an external TCVCXO at 10.0000MHz as the system clock.

UM11126 Section 1.2 under clock generation says
" Crystal oscillator with an operating frequency of 12 MHz to 32 MHz. Option for 
external clock input (bypass mode) for clock frequencies of up to 24 MHz"

LPC55S6x Data sheet (7.22.1) says
Crystal oscillator with an operating frequency of 1 MHz to 32 MHz. Option for external 
clock input (bypass mode) for clock frequencies of up to 24 MHz

Also
In bypass mode, an external clock (maximum frequency of up to 24 MHz) can also be
connected to XTAL32M_P if XTAL32M_N is left open. External [0 – VH] square signal can
be applied on the XTAL32M_P pin from 0 V to 850 mV.

Playing with the clock configuration tool, I cannot set a crystal value of < 12MHz in "Normal crystal oscillation mode.", however by selecting "External clock input (bypass mode)." mode - I can set it to 10MHz.
I am presuming that external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz 

Is this correct??

ラベル(1)
0 件の賞賛
返信
1 解決策
2,671件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

You are right. external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz.

 

Have a nice day,

Jun Zhang

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
1 返信
2,672件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

You are right. external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz.

 

Have a nice day,

Jun Zhang

タグ(1)
0 件の賞賛
返信