External Clock Frequency range LPC55Sxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External Clock Frequency range LPC55Sxx

Jump to solution
2,617 Views
Watarat
Contributor I

I am unclear as to the range of frequencies that can be applied as an external clock.
I wish to use an external TCVCXO at 10.0000MHz as the system clock.

UM11126 Section 1.2 under clock generation says
" Crystal oscillator with an operating frequency of 12 MHz to 32 MHz. Option for 
external clock input (bypass mode) for clock frequencies of up to 24 MHz"

LPC55S6x Data sheet (7.22.1) says
Crystal oscillator with an operating frequency of 1 MHz to 32 MHz. Option for external 
clock input (bypass mode) for clock frequencies of up to 24 MHz

Also
In bypass mode, an external clock (maximum frequency of up to 24 MHz) can also be
connected to XTAL32M_P if XTAL32M_N is left open. External [0 – VH] square signal can
be applied on the XTAL32M_P pin from 0 V to 850 mV.

Playing with the clock configuration tool, I cannot set a crystal value of < 12MHz in "Normal crystal oscillation mode.", however by selecting "External clock input (bypass mode)." mode - I can set it to 10MHz.
I am presuming that external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz 

Is this correct??

Labels (1)
0 Kudos
Reply
1 Solution
2,611 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

You are right. external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz.

 

Have a nice day,

Jun Zhang

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
2,612 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

You are right. external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz.

 

Have a nice day,

Jun Zhang

Tags (1)
0 Kudos
Reply