Eval board for LPC54606J512BD100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Eval board for LPC54606J512BD100

ソリューションへジャンプ
1,651件の閲覧回数
joshua_hong
Contributor III

Hi,

is there any eval board for LPC54606J512BD100?

or eval board with pin to pin compatible which can replace with LPC54606J512BD100?

thanks in advance!

タグ(1)
0 件の賞賛
返信
1 解決策
1,576件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,577件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------