Eval board for LPC54606J512BD100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eval board for LPC54606J512BD100

Jump to solution
544 Views
joshua_hong
Contributor III

Hi,

is there any eval board for LPC54606J512BD100?

or eval board with pin to pin compatible which can replace with LPC54606J512BD100?

thanks in advance!

Tags (1)
0 Kudos
1 Solution
469 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
470 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Joshua Hong,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an eval board for LPC54606J512BD100?
-- No, there're two eval boards for the LPC546xx series, OM13098 and OM13092.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------