Ethernet Time Stamper

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Time Stamper

806件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JM_Romero on Mon Dec 15 05:04:06 MST 2014
Hi everybody,

I am working in a project where I have to time stamp incoming frames from an Ethernet network and store them in the SD Card.

I have observed that after a random number of frames (1, 71, 235, 177000) the Ethernet module freezes and no further frame is recieved. No Interrupt is generated, and the Ethernet module does not modify any descriptor after this.

The traffic we are monitoring is periodic traffic, with 1 ms between frames at least.

Is this a limitation of the Ethernet module?

Does anybody experienced something similar?

Regards,

José Miguel.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)