Ethernet Time Stamper

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Time Stamper

807 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JM_Romero on Mon Dec 15 05:04:06 MST 2014
Hi everybody,

I am working in a project where I have to time stamp incoming frames from an Ethernet network and store them in the SD Card.

I have observed that after a random number of frames (1, 71, 235, 177000) the Ethernet module freezes and no further frame is recieved. No Interrupt is generated, and the Ethernet module does not modify any descriptor after this.

The traffic we are monitoring is periodic traffic, with 1 ms between frames at least.

Is this a limitation of the Ethernet module?

Does anybody experienced something similar?

Regards,

José Miguel.
Labels (1)
0 Kudos
Reply
0 Replies