Error when reselect debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error when reselect debugging

2,248 次查看
1234567890
Contributor IV

I have the same error on 2 different machines (both Kubuntu 18.04 64 bit, MCUXPresso 10.3.1 and SDK for LPC845 Version 2.5.0:

I abort debugging by clicking the red symbol in the upper menu. Then (doing some other things or even not) I click "Debug" in the Quickstart Panel. Then these windows appear on each other (the right one on top):

pastedImage_1.png

The window in the middle has these "Details":

pastedImage_2.png

Then I have to click "Escape" a few times until all windows have disappeared. Then I can click "Debug" again and it works. Every time.

标签 (1)
0 项奖励
回复
4 回复数

2,148 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Whether you can use some screenshots to introduce the complete debug process.
In further, I was wondering if you try to unplug the board, then plug again, before clicking the debug icon. If not, please give a try.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,148 次查看
1234567890
Contributor IV

Hi,

unplugging the board everytime works, but can't be the solution. The problem occurs every time I quit a debug session by clicking the icon at the top (red rectangle in the middle):pastedImage_1.png

0 项奖励
回复

2,148 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
Firstly, I'd like to suggest you reinstall the NXP LPC11Uxx Debug Probe Driver and firmware ( Attachment is the package of firmware and Windows drivers for LPCXpresso boards with an LPC11U35 debug probe.), then try to debug the LPC845 board again.
In addition, whether you encounter the same phenomenon when you use another Linux OS, likes Ubuntu.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,148 次查看
1234567890
Contributor IV

Hi,

Debug Probe Driver for Linux is not necessary/possible, I think. I replaced the firmware with dd if=....., but the problem is still there. Another Linux is no option for that reason.

So I fitted JP2 and attached my J-Link EDU. The problem disappeared, it's much much faster and I'm happy.

0 项奖励
回复