Error in datasheet for LPC54608 for PIO2_11 (FC5_SCK)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in datasheet for LPC54608 for PIO2_11 (FC5_SCK)

1,195 Views
carstengroen
Senior Contributor II

There is an error in the datasheet for the LPC54608. Table 4 on Page 28 lists PIO2_11. According to the table, FUNC 4 for that pin is FC5_SCK. This is not true, it is FUNC5. FUNC4 should be "reserved" according to the UM page 149.

Labels (1)
1 Reply

1,005 Views
soledad
NXP Employee
NXP Employee

Hi,

We are checking this issue internally. Thank you for your feedback.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------