Error in datasheet for LPC54608 for PIO2_11 (FC5_SCK)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in datasheet for LPC54608 for PIO2_11 (FC5_SCK)

1,192件の閲覧回数
carstengroen
Senior Contributor II

There is an error in the datasheet for the LPC54608. Table 4 on Page 28 lists PIO2_11. According to the table, FUNC 4 for that pin is FC5_SCK. This is not true, it is FUNC5. FUNC4 should be "reserved" according to the UM page 149.

ラベル(1)
1 返信

1,002件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

We are checking this issue internally. Thank you for your feedback.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------