Error in Multi-Rate Timer (MRT) with multiple channel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in Multi-Rate Timer (MRT) with multiple channel

Jump to solution
2,924 Views
hemanthvasista
Contributor IV

Hello ,

I am working on the LPC546xx based device. I tried using Multi-Rate Timer (MRT) with multiple channel.

When I configure either of one channel, they work fine individually.
But when I enable both channel, channel-0 is interrupted at different time and no interrupt is generated on channel-1.

Below is code snippet

    /* mrtConfig.enableMultiTask = false; */
    MRT_GetDefaultConfig(&mrtConfig);

    /* Init mrt module */
    MRT_Init(MRT0, &mrtConfig);

    /* Setup Channel 0 to be repeated */
    MRT_SetupChannelMode(MRT0, kMRT_Channel_0, kMRT_RepeatMode);
    MRT_SetupChannelMode(MRT0, kMRT_Channel_1, kMRT_RepeatMode);

    /* Enable timer interrupts for channel 0 */
    MRT_EnableInterrupts(MRT0, kMRT_Channel_0, kMRT_TimerInterruptEnable);
    MRT_EnableInterrupts(MRT0, kMRT_Channel_1, kMRT_TimerInterruptEnable);

    /* Enable at the NVIC */
    EnableIRQ(MRT0_IRQn);

    MRT_StartTimer(MRT0, kMRT_Channel_0, 22000);       //100us interrupt
    MRT_StartTimer(MRT0, kMRT_Channel_1, 220000); //1ms interrupt

The ISR is as below:

void MRT0_IRQHandler(void)
{
    if(MRT_GetStatusFlags(MRT0, kMRT_Channel_0))
    {
        MRT_ClearStatusFlags(MRT0, kMRT_Channel_0, kMRT_TimerInterruptFlag);
        APP_LED_TOGGLE;
    }
    else if (MRT_GetStatusFlags(MRT0, kMRT_Channel_1))
    {
        MRT_ClearStatusFlags(MRT0, kMRT_Channel_1, kMRT_TimerInterruptFlag);
        APP_LED_TOGGLE_1;
    }

/* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping
  exception return operation might vector to incorrect interrupt */
#if defined __CORTEX_M && (__CORTEX_M == 4U)
    __DSB();
#endif
}

regards,
Hemanth

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
2,833 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Hemanth S

 

When channel 1 interrupts channel 0 also gets the interruption. I suggest you add a counter in the interruption on channel 0, when it reaches 1ms, the interruption of the channel 0 is disabled with "MRT_ClearStatusFlags" in order to enter the interruption of channel 1.

Another thing I can suggest is to do this comparison in the "if" sentence

If( 0x3 == MRT_GetStatusFlags(MRT0, kMRT_Channel_0) )

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

View solution in original post

2 Replies
2,834 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Hemanth S

 

When channel 1 interrupts channel 0 also gets the interruption. I suggest you add a counter in the interruption on channel 0, when it reaches 1ms, the interruption of the channel 0 is disabled with "MRT_ClearStatusFlags" in order to enter the interruption of channel 1.

Another thing I can suggest is to do this comparison in the "if" sentence

If( 0x3 == MRT_GetStatusFlags(MRT0, kMRT_Channel_0) )

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

2,833 Views
hemanthvasista
Contributor IV

Thanks for you inputs Omar.

Add of the below line solved the issue:

If( 0x3 == MRT_GetStatusFlags(MRT0, kMRT_Channel_0) )

regards,

Hemanth

0 Kudos
Reply