Entering ISP Mode from user code, LPC54608

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Entering ISP Mode from user code, LPC54608

1,576 Views
patrickhudson
Contributor III

Hello,

Is there an app note or sample code that details entering ISP USB MSC mode from user code in the LPC54608?

The desire is to initiate reprogramming the user application in the LPC54608 flash while the user application is running but without the need to push buttons on the ISP lines (as the product will be packaged, thus no access to isp push buttons).

Thank You,

Patrick

Labels (3)
1 Reply

1,362 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Patrick Hudson,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Unfortunately, I'm afraid that the LPC54608 support this implementation.

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
0 Kudos
Reply