Enable the clock signal for the GPIO.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable the clock signal for the GPIO.

1,581 Views
jameshoho
Contributor I

How do i enable clock signal for GPIO port in LPC1769?? I am new to this board.

I will like to generate a clock signal into P0.27 . I try to generate the clock into this pin but when i read the pin value it read only a value 1. please help thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,206 Views
soledad
NXP Employee
NXP Employee

Hello James,

You can try using the LPCOpen periph_blinky example application for the LPCXpresso1769 board. You can download LPCOpen from LPCOpen Software for LPC17XX|NXP 

I hope this helps,

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply