EVB-4357: project periph_ccan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EVB-4357: project periph_ccan

Jump to solution
2,696 Views
andreaskneissl
Contributor II

In this project an acceptance filter is set to identifier 0x100 and the interrupt filter is handling status interrupts and error interrupts. When I am sending messages with other identifiers, I get an status interupt with status CCAN_STAT_RXOK. But the message I cannot read. When I remove status interrupt from my interrupt filter I get only interrupts for the identifier 0x100, what I expect.

1) Is there any way to get the message of identifier, which are not defined in a filter?
   -> status interrupt CCAN_STAT_RXOK -> read message from other identifier

2) How I can get every message received from the CAN-bus (no filter)

Labels (2)
0 Kudos
Reply
1 Solution
2,406 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andreas Kneissl,

  You can configure the can in the test mode, and enable the basic mode.

   Please modify the code like this:

CCAN_MSG_OBJ_T can_msg;

void CAN0_IRQHandler(void)
{
     CCAN_MSG_OBJ_T msg_buf;
     uint32_t can_int, can_stat, i;
     while ( (can_int = Chip_CCAN_GetIntID(LPC_C_CAN0)) != 0 ) {
          //if ((can_int & CCAN_INT_STATUS) ) 
                if ((CCAN_INT_STATUS == can_int) && (CCAN_STAT_RXOK & LPC_C_CAN0->STAT))
                {
                  //CCAN_MSG_OBJ_T can_msg;

                  can_msg.id = (uint32_t) (LPC_C_CAN0->IF[1].ARB1 | LPC_C_CAN0->IF[1].ARB2 << 16);

                  if (can_msg.id & (0x1 << 30)){
                     can_msg.id &= CCAN_MSG_ID_EXT_MASK;
                    }
                  else {
                     can_msg.id >>= 18;
                     can_msg.id &= CCAN_MSG_ID_STD_MASK;
                   }

                  can_msg.dlc = (uint8_t) (LPC_C_CAN0->IF[1].MCTRL & CCAN_IF_MCTRL_DLC_MSK);

                  *((uint16_t *)&can_msg.data[0]) = (uint16_t) (LPC_C_CAN0->IF[1].DA1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[2]) = (uint16_t) (LPC_C_CAN0->IF[1].DA2 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[4]) = (uint16_t) (LPC_C_CAN0->IF[1].DB1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[6]) = (uint16_t) (LPC_C_CAN0->IF[1].DB2 & 0x0000FFFF);

                 
                  DEBUGOUT("can_msg ID :%x\r\n", can_msg.id);
                    DEBUGOUT("can_msg data :");
                    for (i = 0; i < can_msg.dlc; i++) {
                         DEBUGOUT("%x ", can_msg.data[i]);
                    }
                    DEBUGOUT("\r\nFeed back...\r\n");
                  Rx_Flag =1;
                  LPC_C_CAN0->STAT = LPC_C_CAN0->STAT & (~CCAN_STAT_RXOK);

                  return;
                }

     }
}
int main(void)
{
     CCAN_MSG_OBJ_T send_obj;
     SystemCoreClockUpdate();
     Board_Init();
     set_pinmux();
     DEBUGOUT(WelcomeMenu);
     /* Set CCAN peripheral clock under 100Mhz for working stable */
     Chip_Clock_SetBaseClock(CLK_BASE_APB3, CLKIN_IDIVC, true, false);
     Chip_CCAN_Init(LPC_C_CAN0);
        Chip_CCAN_EnableTestMode(LPC_C_CAN0);//jjadd
       // Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));//jjadd //CCAN_TEST_SILENT_MODE |
     Chip_CCAN_SetBitRate(LPC_C_CAN0, 500000);
     Chip_CCAN_EnableInt(LPC_C_CAN0, (CCAN_CTRL_IE | CCAN_CTRL_SIE | CCAN_CTRL_EIE));

     send_obj.id = CCAN_TX_MSG_ID;
     send_obj.dlc = 4;
     send_obj.data[0] = 'A';
     send_obj.data[1] = 'B';
     send_obj.data[2] = 'C';
     send_obj.data[3] = 'D';
     Chip_CCAN_Send(LPC_C_CAN0, CCAN_MSG_IF1, false, &send_obj);
     Chip_CCAN_ClearStatus(LPC_C_CAN0, CCAN_STAT_TXOK);


        Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));
        
     NVIC_EnableIRQ(C_CAN0_IRQn);

     while (1) {
        
        }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

After modify like the above code, I can receive all the IDs.

The test result is:

pastedImage_1.png

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,407 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andreas Kneissl,

  You can configure the can in the test mode, and enable the basic mode.

   Please modify the code like this:

CCAN_MSG_OBJ_T can_msg;

void CAN0_IRQHandler(void)
{
     CCAN_MSG_OBJ_T msg_buf;
     uint32_t can_int, can_stat, i;
     while ( (can_int = Chip_CCAN_GetIntID(LPC_C_CAN0)) != 0 ) {
          //if ((can_int & CCAN_INT_STATUS) ) 
                if ((CCAN_INT_STATUS == can_int) && (CCAN_STAT_RXOK & LPC_C_CAN0->STAT))
                {
                  //CCAN_MSG_OBJ_T can_msg;

                  can_msg.id = (uint32_t) (LPC_C_CAN0->IF[1].ARB1 | LPC_C_CAN0->IF[1].ARB2 << 16);

                  if (can_msg.id & (0x1 << 30)){
                     can_msg.id &= CCAN_MSG_ID_EXT_MASK;
                    }
                  else {
                     can_msg.id >>= 18;
                     can_msg.id &= CCAN_MSG_ID_STD_MASK;
                   }

                  can_msg.dlc = (uint8_t) (LPC_C_CAN0->IF[1].MCTRL & CCAN_IF_MCTRL_DLC_MSK);

                  *((uint16_t *)&can_msg.data[0]) = (uint16_t) (LPC_C_CAN0->IF[1].DA1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[2]) = (uint16_t) (LPC_C_CAN0->IF[1].DA2 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[4]) = (uint16_t) (LPC_C_CAN0->IF[1].DB1 & 0x0000FFFF);
                  *((uint16_t *)&can_msg.data[6]) = (uint16_t) (LPC_C_CAN0->IF[1].DB2 & 0x0000FFFF);

                 
                  DEBUGOUT("can_msg ID :%x\r\n", can_msg.id);
                    DEBUGOUT("can_msg data :");
                    for (i = 0; i < can_msg.dlc; i++) {
                         DEBUGOUT("%x ", can_msg.data[i]);
                    }
                    DEBUGOUT("\r\nFeed back...\r\n");
                  Rx_Flag =1;
                  LPC_C_CAN0->STAT = LPC_C_CAN0->STAT & (~CCAN_STAT_RXOK);

                  return;
                }

     }
}
int main(void)
{
     CCAN_MSG_OBJ_T send_obj;
     SystemCoreClockUpdate();
     Board_Init();
     set_pinmux();
     DEBUGOUT(WelcomeMenu);
     /* Set CCAN peripheral clock under 100Mhz for working stable */
     Chip_Clock_SetBaseClock(CLK_BASE_APB3, CLKIN_IDIVC, true, false);
     Chip_CCAN_Init(LPC_C_CAN0);
        Chip_CCAN_EnableTestMode(LPC_C_CAN0);//jjadd
       // Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));//jjadd //CCAN_TEST_SILENT_MODE |
     Chip_CCAN_SetBitRate(LPC_C_CAN0, 500000);
     Chip_CCAN_EnableInt(LPC_C_CAN0, (CCAN_CTRL_IE | CCAN_CTRL_SIE | CCAN_CTRL_EIE));

     send_obj.id = CCAN_TX_MSG_ID;
     send_obj.dlc = 4;
     send_obj.data[0] = 'A';
     send_obj.data[1] = 'B';
     send_obj.data[2] = 'C';
     send_obj.data[3] = 'D';
     Chip_CCAN_Send(LPC_C_CAN0, CCAN_MSG_IF1, false, &send_obj);
     Chip_CCAN_ClearStatus(LPC_C_CAN0, CCAN_STAT_TXOK);


        Chip_CCAN_ConfigTestMode(LPC_C_CAN0, ( CCAN_TEST_BASIC_MODE));
        
     NVIC_EnableIRQ(C_CAN0_IRQn);

     while (1) {
        
        }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

After modify like the above code, I can receive all the IDs.

The test result is:

pastedImage_1.png

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply