EEPROM write endurance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM write endurance

Jump to solution
2,174 Views
vaclavrojik
Contributor II

Hello,

I have question about LPC11U24 on-chip EEPROM endurance. Value of parameter is per byte, or per 64B page?

When I wrote one byte to adress 0x0000, I shorted life for next 63 bytes in page, or not?

Thank You

Vaclav

Labels (1)
0 Kudos
Reply
1 Solution
1,978 Views
soledad
NXP Employee
NXP Employee

Hi,

When a single byte is programmed, the energy from the charge pump is concentrated on that one byte. If a page write is used, that energy is dissipated over more bytes, so cell wear is decreased.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,979 Views
soledad
NXP Employee
NXP Employee

Hi,

When a single byte is programmed, the energy from the charge pump is concentrated on that one byte. If a page write is used, that energy is dissipated over more bytes, so cell wear is decreased.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------