Dual Core Release debugging with PE Micro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Core Release debugging with PE Micro

Jump to solution
2,534 Views
DanielR
Contributor I

I am using the LPCXPRESSO LPC54102 EVAL BRD (OM13077UL) for developing a dual core project on the LPC54102. I have discovered that when I build my code in Release mode, I am no longer able to use the PE Micro Multi Link probe (connected via SWD)

When I try to launch the debugger, the master image loads fine, but then I get the following error when it tries to load and launch the slave image:

DanielR_0-1663784435442.pngDanielR_0-1663784435442.png

The PE Micro probe works in Debug mode and the J Link probe built into the eval board works fine in both Debug and Release mode. This is a problem, because in my final product, I will not have the built in J Link probe, I will only have the SWD port. Is this a limitation of SWD or the PE Micro?

 

Thank you,

   Daniel

 

Labels (1)
0 Kudos
Reply
1 Solution
2,511 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing. 

It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder  .metadata under workspace to try. 

 

BR

Alice

View solution in original post

0 Kudos
Reply
2 Replies
2,520 Views
DanielR
Contributor I

I am not sure what I was doing wrong yesterday. I did a clean and full compile on the Master and Slave and now the PE Micro probe seems to be working fine. I would still like to know what was causing the error yesterday.

0 Kudos
Reply
2,512 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing. 

It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder  .metadata under workspace to try. 

 

BR

Alice

0 Kudos
Reply