Dual Core Release debugging with PE Micro

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual Core Release debugging with PE Micro

跳至解决方案
2,714 次查看
DanielR
Contributor I

I am using the LPCXPRESSO LPC54102 EVAL BRD (OM13077UL) for developing a dual core project on the LPC54102. I have discovered that when I build my code in Release mode, I am no longer able to use the PE Micro Multi Link probe (connected via SWD)

When I try to launch the debugger, the master image loads fine, but then I get the following error when it tries to load and launch the slave image:

DanielR_0-1663784435442.png

The PE Micro probe works in Debug mode and the J Link probe built into the eval board works fine in both Debug and Release mode. This is a problem, because in my final product, I will not have the built in J Link probe, I will only have the SWD port. Is this a limitation of SWD or the PE Micro?

 

Thank you,

   Daniel

 

标签 (1)
0 项奖励
回复
1 解答
2,691 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing. 

It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder  .metadata under workspace to try. 

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,700 次查看
DanielR
Contributor I

I am not sure what I was doing wrong yesterday. I did a clean and full compile on the Master and Slave and now the PE Micro probe seems to be working fine. I would still like to know what was causing the error yesterday.

0 项奖励
回复
2,691 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing. 

It's hard to know exactly where the problem is, and yes, clean and compile is the commonly used method, also can delete folder  .metadata under workspace to try. 

 

BR

Alice

0 项奖励
回复