Drop in replacement for OM13056

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drop in replacement for OM13056

4,430件の閲覧回数
thomaspeter-volpi
Contributor II

Hi

We are trying to get a hold of a few OM13056 LPCXpresso boards (8 units max.), but none of the big distributors have it in stock.  

Is there maybe a drop-in replacement for the OM13056 available? We have a custom PBC that is plugged onto the header sockets of an OM13056 and we would like to reproduce that setup.

Best regards 

Thomas

 

ラベル(1)
タグ(1)
8 返答(返信)

4,366件の閲覧回数
thomaspeter-volpi
Contributor II

Hi XiangJun 

I tried https://www.nxp.com/part/OM13056#/, but the major distributors don't have it in stock. I also don't need a drop in replacement for the board and its headers, not the chip LPC1549JBD64. If there is another LPCXpresso board with the same header interface that can run the same software as the OM13056 I would be happy with that.

Best regards

Thomas

0 件の賞賛
返信

4,359件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you just use Arduino header, it is okay, a lot of board has the Arduino header.

Can you tell us the header signals you are using?

BR

XiangJun Rong

0 件の賞賛
返信

4,350件の閲覧回数
thomaspeter-volpi
Contributor II

Arduino.pngThis is how we use the Arduino header interface.

I suppose the OM13058 would work (https://www.nxp.com/part/OM13058#/), but I don't know how much we would have to change the firmware that was written for the OM13056 to be running on the OM13058. Or would it be pretty straightforward to port a firmware for the OM13056 to the OM13058?

0 件の賞賛
返信

4,307件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If the connector signals match between OM13056 and OM13058, porting the firmware is not a huge task, because all the code is written with C language.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

4,345件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The OM13058 is based on LPC11U68, which uses Cortex-M0 core.

If you have the source code and just use GPIO, uart, ADC, I do not think the task is huge.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

4,327件の閲覧回数
thomaspeter-volpi
Contributor II

Hi

Is there another NXP MCU DevKit with Arduino headers that uses an ARM Cortex-M3 microcontroller?

Best regards

Thomas

0 件の賞賛
返信

4,317件の閲覧回数
frank_m
Senior Contributor III

Other vendors like ST have Arduino-compatible headers as well.
Like most of their Discover and Nucleo boards.
However, I consider their "Cube" library/SDK a regular disaster.

0 件の賞賛
返信

4,399件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the OM13056 board, it is also called LPCXpresso1549, which uses LPC1549JBD64 processor.

I suppose that there is not Drop in replacement for LPC1549JBD64 

It appears that you can order the silicon  from the link:

https://www.nxp.com/part/LPC1549JBD64#/

For the OM13056 board ordering, pls try the website:

https://www.nxp.com/part/OM13056#/

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信