Drop in replacement for LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Drop in replacement for LPC546xx

Jump to solution
2,084 Views
evan_ohlsen
Contributor II

The product I am working on uses an LPC54618J512ET180E. I noticed that recently, the LPC54628 was released and has the same TFBGA-180 package. From the datasheets it looks like the 54628 is a drop-in-replacement for the 54618. Is this true? If the pinout is the same, can I safely port software from the 54618 to the 54628 without needing to rewrite peripheral and IO drivers?

Additional information on the lifespan of the LPC54618J512ET180E package would be helpful as well.

 

Thank you,

Evan

Labels (4)
0 Kudos
Reply
1 Solution
2,067 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

". Is this true? "

->> Yes,LPC54628 is a drop-in-replacement for the LPC54618.

"Additional information on the lifespan of the LPC54618J512ET180E"

->> The longevity years of LPC546xx is 15, until Dec 2031.

Alice_Yang_0-1615962767062.png

 

BR

Alice

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
2,068 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

". Is this true? "

->> Yes,LPC54628 is a drop-in-replacement for the LPC54618.

"Additional information on the lifespan of the LPC54618J512ET180E"

->> The longevity years of LPC546xx is 15, until Dec 2031.

Alice_Yang_0-1615962767062.png

 

BR

Alice

 

 

 

0 Kudos
Reply