Drop in replacement for LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drop in replacement for LPC546xx

ソリューションへジャンプ
2,077件の閲覧回数
evan_ohlsen
Contributor II

The product I am working on uses an LPC54618J512ET180E. I noticed that recently, the LPC54628 was released and has the same TFBGA-180 package. From the datasheets it looks like the 54628 is a drop-in-replacement for the 54618. Is this true? If the pinout is the same, can I safely port software from the 54618 to the 54628 without needing to rewrite peripheral and IO drivers?

Additional information on the lifespan of the LPC54618J512ET180E package would be helpful as well.

 

Thank you,

Evan

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
2,060件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

". Is this true? "

->> Yes,LPC54628 is a drop-in-replacement for the LPC54618.

"Additional information on the lifespan of the LPC54618J512ET180E"

->> The longevity years of LPC546xx is 15, until Dec 2031.

Alice_Yang_0-1615962767062.png

 

BR

Alice

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,061件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

". Is this true? "

->> Yes,LPC54628 is a drop-in-replacement for the LPC54618.

"Additional information on the lifespan of the LPC54618J512ET180E"

->> The longevity years of LPC546xx is 15, until Dec 2031.

Alice_Yang_0-1615962767062.png

 

BR

Alice

 

 

 

0 件の賞賛
返信