Driving LPC2131 VDD above the Absolute Maximum Rating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driving LPC2131 VDD above the Absolute Maximum Rating

961件の閲覧回数
sylvainpoulin
Contributor I

Hi,

We have been using the LPC2131 in our design for years and driving it (VDD) at 3.3V. We just realized that our board voltage monitoring circuit would not triggered an error until the voltage goes above 3.9V for VDD.

As of safety concern, what would happen to the device if it would be feed at 3.9V instead of 3.3V ?

Would it catch into fire or it would only reduce its MTBF and affect its behavior/performance ?

Thanks in advance !

0 件の賞賛
返信
1 返信

885件の閲覧回数
art
NXP Employee
NXP Employee

Q. Would it catch into fire or it would only reduce its MTBF?

A. There is no definite answer to this question. Both cases are possible.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信