Driving LPC2131 VDD above the Absolute Maximum Rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driving LPC2131 VDD above the Absolute Maximum Rating

967 Views
sylvainpoulin
Contributor I

Hi,

We have been using the LPC2131 in our design for years and driving it (VDD) at 3.3V. We just realized that our board voltage monitoring circuit would not triggered an error until the voltage goes above 3.9V for VDD.

As of safety concern, what would happen to the device if it would be feed at 3.9V instead of 3.3V ?

Would it catch into fire or it would only reduce its MTBF and affect its behavior/performance ?

Thanks in advance !

0 Kudos
Reply
1 Reply

891 Views
art
NXP Employee
NXP Employee

Q. Would it catch into fire or it would only reduce its MTBF?

A. There is no definite answer to this question. Both cases are possible.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply