Does a TF-M sample exist for LPC55S69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does a TF-M sample exist for LPC55S69

Jump to solution
3,684 Views
danielbujak
Contributor III

I'm looking to run the TF-M project on the LPC55S69. Is there any such example project to take advantage of the ARMv8 architecture?

0 Kudos
Reply
1 Solution
3,392 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

You're right, this examples aren't generated in the MCUXpresso version. I will report this to our SDK team.

Best Regards,
Alexis Andalon

View solution in original post

4 Replies
3,392 Views
danielbujak
Contributor III

So I've discovered that if I generate the SDK for Keil uVision then a TF-M application is generated, however without mcu-boot which is part of the TF-M application. That leaves me with 2 questions:

1. Should / will mcuXpresso support this example?

2. Is there a BL2 sample implementation available?

0 Kudos
Reply
3,392 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

If you're refering to the Trustzone examples, that ones are also supported in MCUXpresso. Also, what do you mean with with BL2?

Best Regards,

Alexis Andalon

0 Kudos
Reply
3,392 Views
danielbujak
Contributor III

Hi Alexis,

1.Okay thanks, it seems like this may be a bug with the SDK generator then, since the project is only packaged when using uVision

2. BL2= 2nd stage bootloader. TF-M uses mcuboot for this to do image verification and firmware update ( http://connect.linaro.org.s3.amazonaws.com/hkg18/presentations/hkg18-223.pdf )

Regards,

Daniel

0 Kudos
Reply
3,393 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

You're right, this examples aren't generated in the MCUXpresso version. I will report this to our SDK team.

Best Regards,
Alexis Andalon