Does a TF-M sample exist for LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does a TF-M sample exist for LPC55S69

ソリューションへジャンプ
3,721件の閲覧回数
danielbujak
Contributor III

I'm looking to run the TF-M project on the LPC55S69. Is there any such example project to take advantage of the ARMv8 architecture?

0 件の賞賛
返信
1 解決策
3,429件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

You're right, this examples aren't generated in the MCUXpresso version. I will report this to our SDK team.

Best Regards,
Alexis Andalon

元の投稿で解決策を見る

4 返答(返信)
3,429件の閲覧回数
danielbujak
Contributor III

So I've discovered that if I generate the SDK for Keil uVision then a TF-M application is generated, however without mcu-boot which is part of the TF-M application. That leaves me with 2 questions:

1. Should / will mcuXpresso support this example?

2. Is there a BL2 sample implementation available?

0 件の賞賛
返信
3,429件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

If you're refering to the Trustzone examples, that ones are also supported in MCUXpresso. Also, what do you mean with with BL2?

Best Regards,

Alexis Andalon

0 件の賞賛
返信
3,429件の閲覧回数
danielbujak
Contributor III

Hi Alexis,

1.Okay thanks, it seems like this may be a bug with the SDK generator then, since the project is only packaged when using uVision

2. BL2= 2nd stage bootloader. TF-M uses mcuboot for this to do image verification and firmware update ( http://connect.linaro.org.s3.amazonaws.com/hkg18/presentations/hkg18-223.pdf )

Regards,

Daniel

0 件の賞賛
返信
3,430件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Daniel,

You're right, this examples aren't generated in the MCUXpresso version. I will report this to our SDK team.

Best Regards,
Alexis Andalon