Differences between LPC43S67 and LPC4367 - significance of "S" ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences between LPC43S67 and LPC4367 - significance of "S" ?

1,527 Views
robotxyz
Contributor I

Hi,

LPC43S67 is supposed to support secure mode. Other than that, are there any differences between LPC43S67 and LPC4367 chip ? Are the pin outs and other functionality the same on these two parts ?

If I develop code on a dev board with LPC43S67, will the code work on a custom designed board with LPC4367 part or vice versa (ignoring the secure mode, since I do not use the secure mode) ?

Thanks,

robot xyz

2 Replies

1,446 Views
bernhardfink
NXP Employee
NXP Employee

LPC4367 code will work on the LPC43S67 and vice versa, as long as you don't use the AES engine feature.

The devices are identical , in the non-S version the AES engine is disabled.

Regards,

Bernhard.

1,446 Views
robotxyz
Contributor I

Thanks Bernhard.

0 Kudos
Reply