Differences between LPC43S67 and LPC4367 - significance of "S" ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differences between LPC43S67 and LPC4367 - significance of "S" ?

1,496件の閲覧回数
robotxyz
Contributor I

Hi,

LPC43S67 is supposed to support secure mode. Other than that, are there any differences between LPC43S67 and LPC4367 chip ? Are the pin outs and other functionality the same on these two parts ?

If I develop code on a dev board with LPC43S67, will the code work on a custom designed board with LPC4367 part or vice versa (ignoring the secure mode, since I do not use the secure mode) ?

Thanks,

robot xyz

2 返答(返信)

1,415件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

LPC4367 code will work on the LPC43S67 and vice versa, as long as you don't use the AES engine feature.

The devices are identical , in the non-S version the AES engine is disabled.

Regards,

Bernhard.

1,415件の閲覧回数
robotxyz
Contributor I

Thanks Bernhard.

0 件の賞賛
返信